Licensing a Database Instance

Each database instance requires a license, just like any other ClearSCADA database server. When you have purchased a license for a database instance, you will need to use the Server Icon to associate the license with the instance:

  1. Run the Server Icon for a Database Instance
  2. Right-click on the server icon and choose the License Details option.
    The License Details <Database Instance Name> window is displayed.
  3. Use the Change button to browse to the License for the database instance.
  4. Select the Close button.

The license settings are detected by the database instance automatically (as long as the database instance can locate the license file or detect the dongle in a parallel port or USB port).

Further Information

License Details: see Understanding the License Details Window in the ClearSCADA Guide to Server Administration.


Disclaimer

ClearSCADA 2017 R2